DRV.BOOTTIME
Description
DRV.BOOTTIME returns the time that the current session started running.This time includes total amount of time from all previous sessions.
This keyword can be used with DRV.RUNTIME to determine the length of time the drive has been running since it was last power cycled.
Session Time = DRV.RUNTIME – DRV.BOOTTIME
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
Days:Hours:Minutes:Seconds |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
String |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Related Topics